Cancel
Showing results for 
Search instead for 
Did you mean: 

Installation problems Mac OS X 10.10.5

Experimenter
Experimenter

Hey everyone,

 

I'm using NX11.0 for my study. After hours of trying to install NX11 on my MacBook Pro I'm asking you for help. I already installed XQuartz and Java on my Mac. After completing the installation of NX11 I tried to run NX. NX showed after a few second it's startup screen but it shutdown directly after that. I tried to restart my Mac but it didn't solve the problem. I hope that anyone here can help me.

 

8 REPLIES

Re: Installation problems Mac OS X 10.10.5

Siemens Experimenter Siemens Experimenter
Siemens Experimenter

Hi Benny,

 

you failed to mention on which Mac OS version you've installed NX11.

Also do mention which XQuartz version you've installed, I noticed that XQuartz 2.7.10 and 2.7.11 cause NX11 to NOT start on “El Capitan” and “Sierra”, with XQuartz 2.7.9 it works fine.

 

P.S. I couldn't see your movie.

 

Kind regards,

Aurelio Martinez

 

Re: Installation problems Mac OS X 10.10.5

Siemens Experimenter Siemens Experimenter
Siemens Experimenter

Hi Benny,

 

sorry, it's in the header, Mac OS X 10.10.5, so please check the XQuartz version first.

 

Kind regards,

Aurelio Martinez

 

Re: Installation problems Mac OS X 10.10.5

Experimenter
Experimenter

Hi Aurelio

Thank you so much for your help. After the installation of the correct XQuartz version NX11 works well !!

Re: Installation problems Mac OS X 10.10.5

Experimenter
Experimenter

Re: Installation problems Mac OS X 10.10.5

Siemens Experimenter Siemens Experimenter
Siemens Experimenter

Yes, I know, this is the Documentation for NX.

Here you can also find the information for other NX versions, supported platforms, etc.

 

Thanks anyway.

 

Kinde regards,

Aurelio

Re: Installation problems Mac OS X 10.10.5

Creator
Creator

Hey,

 

How did you installed NX11 ? I'm getting mad with that... we got a uni. license but I don't know how to use the script. ug_install... 

 

 

Re: Installation problems Mac OS X 10.10.5

Siemens Experimenter Siemens Experimenter
Siemens Experimenter

Hi,

 

on Yosemite you first need to install XQuartz version 2.7.9 (beware, v2.7.10 and 2.7.11 don't work with NX).

 

Depending on the license file you have, you need to install the SPLM License Server (server license),

or just point to the license file (node-locked license) during NX installation.

 

For NX11 :

 

  • Run “nx110.mpkg” to do the installation
  • Accept the “28000@servername” entry to the License Server, or browse to the license file
  • License Tools --> Bundles are available and can be chosen
    Applications - Siemens – NX11.0 Apps - NX Licensing Tools - Licensing Tool

Start NX11.0 --> Applications - Siemens – NX11.0 Apps – NX11.0

Hereafter you can also install Maintenance Release NX11.0.2.7

 

Kind regards,

Aurelio Martinez

 

Re: Installation problems Mac OS X 10.10.5

Creator
Creator

Thx, I will try after my exams, and I'll update the result!

 

It's for a 2Q course and all mac users we have the same probleme, no easy guide as you can find for windows, and i dont wanna devide my SSD to install W10.