Cancel
Showing results for 
Search instead for 
Did you mean: 
Highlighted

Interpart Expressions NX8.5-NX11 units conversion

Creator
Creator

We are preparing to transition to NX11 from NX8.5. I am working in native...

 

I have read thru the posts on the new way for interpart expressions but have a different issue with them.

 

When I open my NX8.5 part in NX11 it creates the "*_0" interparts for me but I get an error message:

 

error.jpg

But they did match in NX8.5, they were both constant in the child and parent (source) part files:

source.jpg

parent.jpg

 

Now it is making my "*_0" new expressions as Length and I can't edit them to make them Constant:

exp_list.jpg

 

Is there a setting I can change or a way to edit these to be Constant that I am not seeing?

I don't want to change the original exp's to Length

thanks

5 REPLIES

Re: Interpart Expressions NX8.5-NX11 units conversion

Solution Partner Phenom Solution Partner Phenom
Solution Partner Phenom
you can select the cells in the expressions dialog and copy them into Excel.

here you can quickly remove the *_0 by using the replace tool.
then copy everything back into the expressions dialog.

Ruud van den Brand
Pre-sales NX CAD
cards PLM Solutions

Re: Interpart Expressions NX8.5-NX11 units conversion

Creator
Creator

But those are the interpart expressions that the system automatically generates when it updates the 8.5 part file to 11...I have to keep those right?

I just want to change the "Dimensionality" of the *_0 expressions from Length to Constant

Re: Interpart Expressions NX8.5-NX11 units conversion

Solution Partner Phenom Solution Partner Phenom
Solution Partner Phenom

if i look into your pictures. do you have create for your self again the one that you need or did NX creates the both 


Ruud van den Brand
Pre-sales NX CAD
cards PLM Solutions

Re: Interpart Expressions NX8.5-NX11 units conversion

Creator
Creator
NX created the _0 expressions. The other ones were already there in my NX8.5 file. I didn't create any new expressions

Re: Interpart Expressions NX8.5-NX11 units conversion

Creator
Creator

This has been resolved in version 11.0.2. The error message does not come up anymore.

Thank you Scott @ GTAC...ref IR#9026360