01-18-2017 08:12 AM
01-18-2017 11:36 AM
Hello @DC1,
I have just tried this in NX 9.0.3 MP15 and here it seems to work just fine. Not sure if this is a bug in a previous version or not? But apparently not a general issue.
Kind regards,
Dennis
01-19-2017 06:34 AM
Hello Dennis,
Our version is the same as yours. I'll have to have a look in the settings. I'll re-post if I can find
anything out.
Thanks for the reply
Best regards
Dave Clark
01-19-2017 07:41 AM
Hello @DC1,
Just so you know, What I tested was create, 1 part, and add 3 Bodies in this part,
Create a new drawing (master-model). Add a view on this drawing, do the view dependend edit, select one body, and do the invert selection. This works fine for me.
Not sure if this is the same setup you use? or do you create the drawing of an assembly?
Kind regards,
Dennis
01-19-2017 01:06 PM
Could be dialog memory is doing something?
Production: NX10.0.3.5 MP16/TC11.2
I'd rather be e-steamed than e-diseaseled
01-20-2017 03:41 AM
Hello,
Just to let you know my situation:
I have produced my model assembly in modelling and switched to drafting mode.
Placed the views I required on the drawing sheets. Sheet 1 has the assembly views with parts list.
On the following sheets I normally place the individual parts of the assembly with dimensions for manufacture.
This was done in NX7.5 by placing the full assembly view on the sheet using the "base view" button. Next is to right click on the view and select "View dependent edit", select the "erase objects" button in the "add edits" box, select the body in the view that I want to keep and click the "invert selection" button in the "class selection" window. This used to leave the part that I want to dimension in the view but in NX9 it keeps all items selected and erases all parts from the view.
I now tend to use layers more to just leave the part required in the view by using the "layers visible in view" button.
Thanks for replies
Dave Clark
01-20-2017 08:35 AM
Here are a couple of alternatives to using the "view dependent edit" command:
01-20-2017 09:10 AM
Hello cowski1,
Thanks for your reply.
I do add component parts to an assembly draft but I find that this adds an extra body to the assembly.
This isn't a problem generally but I have to prepare an export file for manufacturing and this extra body shows up in the export file if I select all parts in the assembly, unless I only select the parts that I require.
I can get round things but it just seemed to be easier in NX7.5.
I haven't used the "hide component in view " so I'll have a play around with that.
Thanks again.
Dave
01-20-2017 09:25 AM
Adding a view from another part (i.e. using a "drafting component") will NOT add another body to your assembly. When adding a base view, in the "select part" step (top of the dialog), select your piece part of interest and specify which model view and scale to use. This will add a view (and only a view) of that part to your drawing; the view will be generated from the part file (not the assembly) and as such will not have the other assembly components in it. Instead of the normal "yellow cube" icon that represents a component, it will be a "yellow cube on top of a drawing" icon, indicating a drafting component. Nothing new will show up in the modeling application nor will it affect your parts list.