Cancel
Showing results for 
Search instead for 
Did you mean: 

Re: Is NX9 Dimensioning a step forward?

Experimenter
Experimenter

Dave,

Please include me for the webinar.


Time Zone: Eastern

 

Currently using NX 9.

 

Thanks

Jeremy

NX 8.5 NX 9.02 Catia V5

Re: Is NX9 Dimensioning a step forward?

Phenom
Phenom
Another limitation is Lower case tolerance with Rapid Dimension in NX 9 aren't present.
You have to edit the dimension.
Step 1: Double-click to Edit Dimension
Step 2: Select Text Settings Button on Scene Dialog
Step 3: Change to the appropriate Hole / Shaft option
Step 4: Once “Shaft” is selected, the lower case options are available on the Settings UI and in the Scene Dialog
Thank you...

Using NX11 and NX1847
RuleDesigner PDM

Re: Is NX9 Dimensioning a step forward?

Genius
Genius
As far as I know this will be fixed in NX10 - good for those customer who want to skip NX9...
I hope there is no showstopper in NX10 because we aim to that release...

Re: Is NX9 Dimensioning a step forward?

Pioneer
Pioneer

Hi Dave,

 

I too would like to participate in the webinar

 

Timezone AEDT Sydney, Australia (UTC+11.00)

 

Thanks,

Geoff

Geoff Donohoo

NX10.0.3.5 & TC 10.1.4.2
Dell T3600 32Gb Ram, Nvidia Quadro 4000
Windows 7

Re: Is NX9 Dimensioning a step forward?

Gears Phenom Gears Phenom
Gears Phenom

Thanks Dave for holding This webinar. 

Re: Is NX9 Dimensioning a step forward?

Valued Contributor
Valued Contributor

Yes. Thanks Dave.

SteveA
DRT Mfg. Co. Inc.
www.drtusa.com
Win7x64 NX8.5.3.3

Re: Is NX9 Dimensioning a step forward?

Legend
Legend

Did the webinar happen?

 

I barely use drafting, I just make some rough "prints" for the guys on the shop floor, not detailed drawings.

 

The advances in syncronous modeling and the addition of "fill surface" and "blend corner" make the jump to NX9 very worthwhile for me. It seems there are some background changes in blending (Face and Edge)as well. Things that would never blend in the past do so with ease now.

Rob Newcomb, CAD/CNC/Simulation manager
Elmhirst Industries, Specializing in Prototype sheet metal stampings and assemblies

Production: NX 12.0.2 / Autoform r7 /WorkNC 2018 r2
Testing:NX EAP
PC: Rave Cadbeast: Intel(R) i7-4790K CPU @ 4.GHz /32gb ram /NVIDIA Quadro P2000 on Win10 Pro

Re: Is NX9 Dimensioning a step forward?

Valued Contributor
Valued Contributor

So what was the outcome of the webinar? Has it been held yet?

Will it be hosted somewhere so it can viewed by those who coludnt make it?

NX9 has brought some nice changes but there is some polish required still.

Regards

Adrian

Re: Is NX9 Dimensioning a step forward?

Solution Partner Phenom Solution Partner Phenom
Solution Partner Phenom
Yes it has been held. As to whether it will be hosted somewhere is up to Mr Wingrave to comment.
Anthony Galante, Senior Support Engineer
PhoenxPLM
24 versions of NX installed: NX4 to NX12, plus TC11.2

Re: Is NX9 Dimensioning a step forward?

Valued Contributor
Valued Contributor

Thanks Anthony, was any consensus about the UI reached? Did some of the earlier commenters get clarification/reassurance?

Rgds

Adrian