Cancel
Showing results for 
Search instead for 
Did you mean: 
Highlighted

Is possible export VDA file from UGNX7.5?

Experimenter
Experimenter

Hi All.

 

Does anybody know if is possible export VDA file from UGNX7.5?

 

Thank you

9 REPLIES

Re: Is possible export VDA file from UGNX7.5?

Siemens Phenom Siemens Phenom
Siemens Phenom

Are you taking about VDA-FS?  If so, that's an obsolete surface-only exchange standard that has since been superseded by STEP, which NX 7.5 does support.

John R. Baker, P.E. (ret)
EX-Product 'Evangelist'
Irvine, CA

Re: Is possible export VDA file from UGNX7.5?

Genius
Genius

Hello

 

in Germany you can buy a VDA interface directly from Siemens,it is an add-on.

I've attached th first pages of the user manuel os you can contact you local NX reseller.

 

And John, no VDA-FS isn't superseded by STEP. There are features included which STEP don't support.

VDA is for example popular for programming CMM machines, and of course for data translation with old fashioned CAD systems like EUCLID.

 

 


Meinolf, , Leistritz Turbinentechnik GmbH


Production: NX10.0.3, TC 10.1.4

Testing:NX11 Beta

Re: Is possible export VDA file from UGNX7.5?

Experimenter
Experimenter

Thank you guys.

 

And this will be the same for NX8.5, yes?

Re: Is possible export VDA file from UGNX7.5?

Also for NX 9.0

Best Regards Michael
CAx Solutions

Re: Is possible export VDA file from UGNX7.5?

Siemens Phenom Siemens Phenom
Siemens Phenom

The site I checked stated that VDA-FS was superceded by STEP.  That was all that I had to go by.

John R. Baker, P.E. (ret)
EX-Product 'Evangelist'
Irvine, CA

Re: Is possible export VDA file from UGNX7.5?

Experimenter
Experimenter

Hi.

 

I have already recieved licence from Siemens for VDA export. But... Do you know where I can download necessary software (add-in etc)?

 

Thank you

Re: Is possible export VDA file from UGNX7.5?

Genius
Genius
Have you checked the GTAC download area, full product?


Meinolf, , Leistritz Turbinentechnik GmbH


Production: NX10.0.3, TC 10.1.4

Testing:NX11 Beta

Re: Is possible export VDA file from UGNX7.5?

On the GTAC Download server go to "Full Product Download". If you're registered correctly you should get an additional tab "VDAFS" alongside with "NX/Unigraphics NX".

Best Regards Michael
CAx Solutions

Re: Is possible export VDA file from UGNX7.5?

Experimenter
Experimenter

Thank you guys. IT was there. I have just cleared IE cache, and then it appears.

 

Thank you again.