Cancel
Showing results for 
Search instead for 
Did you mean: 

Is there a list of text format keys for Drafting?

Pioneer
Pioneer

Is there a list of formatting keys for text in Drafting?  For example, if I want to increase the size of a portion of text, I would insert <C2.00> to make the text 2 x size and then <C> to get back to normal text size.  What I am looking for in particular is a way to add a "strikethrough" for a portion of text.  But also, if I could get my hands on a complete list of formatting codes, it would be even better.  Thanks.

2 REPLIES 2

Re: Is there a list of text format keys for Drafting?

Honored Contributor
Honored Contributor

In the help files.  I see underline, but not strike thru:

 

https://docs.plm.automation.siemens.com/tdoc/nx/11.0.2/nx_help/#uid:xid1128417:index_drafting:id7008...

-Dave
NX 11 testing NX1847+ | Teamcenter 11 | Windows 10
Highlighted

Re: Is there a list of text format keys for Drafting?

Siemens Phenom Siemens Phenom
Siemens Phenom

Hi @DaveL3149,

As @DaveK pointed, that is the link from NX documentation for list of drafting control characters.

 

For notes created using 'Note' commad, there is no direct option or a way to apply complete or partial strikethrough. However for tabular notes you can apply strikethrough to all or some specific cells using edit spreadsheet option. In this case strikethrough will be applied to complete cell content.