Cancel
Showing results for 
Search instead for 
Did you mean: 

Issue with circle selection method

Phenom
Phenom

NX has a newer selection mode: Circle. Most people use the default rectangle mode. But there are modes for rectangle, lasso and now circle.

I have been showing circle selection to people have found that it has a very, very poor performance.

When I use a multi-select rule that includes the crossing as an option it takes 20-30 seconds for NX to select the parts. There are only 322 components in the entire assembly and the areas I attempt to work on contain, on average 20-30 components.

Using rectangle NX selects, on average, in 2-3 seconds. Lasso is considerably longer at around 10-12 seconds.

 

I'm wondering if anyone else is experiencing similar results.

2 REPLIES 2

Re: Issue with circle selection method

Siemens Phenom Siemens Phenom
Siemens Phenom

Ryan,

I think a PR might be in order. I can see a measurable difference between rectangle and circle.

Regards,
Abe

Re: Issue with circle selection method

Siemens Phenom Siemens Phenom
Siemens Phenom

Have you tried turning off 'Pre-Selection Highlighting' to see if that makes a difference?  If it does, make sure you indicate when talking to GTAC or if and when an IR/PR is opened.

John R. Baker, P.E. (ret)
EX-Product 'Evangelist'
Irvine, CA