Cancel
Showing results for 
Search instead for 
Did you mean: 

It's not activate I-DEAS commands, even if I click icons.

Solution Partner Genius Solution Partner Genius
Solution Partner Genius

Hi, everybody!

 

I'm in trouble with operate I-DEAS.
I was re-installed I-DEAS. But, it is not activate even if I click icons.

 

What's wrong with I-DEAS?
How can I treat this trouble?

 

Please let me know!

 

Thank you!

 

1 REPLY 1

Re: It's not activate I-DEAS commands, even if I click icons.

Siemens Phenom Siemens Phenom
Siemens Phenom

@LittleWillie76:

 

Can you provide a bit more detail?

 

Which version of I-deas? The latest 6.6?

Which OS? Windows 10?

It sounds like you were able to enter a Model File name and start I-deas. Which Application? Design? Simulation? And which Task? Master Modeler?

Now, which command you are trying?

 

To start the basics, get to Appliation=Design, Task=Master Moderer and create a block.

Column 3, Row 9, "Create Part", then Block.

 

To be sure the problem is not with icons, try to menus.

Turn menus on under Options, from the top menu, Menus/On/Off

Then CA-Catalog, P-Parts

Or just type in the Prompt Region: /ca p

 

If none that works, you might have a license problem, although typically you would not even be able to launch to the Master Modeler if that's the case.