Cancel
Showing results for 
Search instead for 
Did you mean: 

It takes a very long time to Open Assembly from NX9.0.3.4 with Teamcenter 10.1 Intergrated

Experimenter
Experimenter

Dear everybody

 

Now I am using NX9.0.3 with Teamcenter 10.1 intergrated

Recently, When I am opening Asscembly (In Assembly Navigator, select assembly >> Open >> Assembly),It takes very long time to retrive and load structure of my assembly.

You can see the operation in photo in attachment

 

I takes over 20 minutes to open assembly (before is about 1.5 minutes).

 

I am using Teamcenter intergrated with 2 FSC servers (one is cache server).

I tried to clear FSC Cache on Cache server but speed value is as slow as before

I checked server performance, it is good (30% used memory, 40% CPU process)

I checked network performance, it is good too

We have about 700 users are using NX

 

So, I dont know how to solve this problem

Does anyone meet this trouble before?

Please give me an advice

 

Thanks !

 

1 REPLY

Re: It takes a very long time to Open Assembly from NX9.0.3.4 with Teamcenter 10.1 Intergrated

Siemens Phenom Siemens Phenom
Siemens Phenom

What the your load options set to? Load options can have a big effect on the time it takes to start working.

 

What does the menu of file -> options -> Load options look like?

 

Thanks,

Scott