Cancel
Showing results for 
Search instead for 
Did you mean: 

Journal editer in NX

Experimenter
Experimenter

Hello,

 

How can i use Journal editer in modelling? could someone explain with an example?

 

Regards

Ganesha C U 

2 REPLIES 2

Re: Journal editer in NX

Siemens Esteemed Contributor Siemens Esteemed Contributor
Siemens Esteemed Contributor
These steps are fairly rudimentary, but they should help to explain the functionality:
a) Open a part in NX and record a journal in modeling while making changes to the part.
b) Undo the commands that the journal recorded and playback the journal (to make sure it functions correctly)
c) Open the Journal Editor and make changes to the journal you just recorded
d) Use the Play button on the Journal Editor to test the changes
e) Save (or Save As) the modified journal

Does that help or do you still need an example?
Regards, Ben


Re: Journal editer in NX

Siemens Phenom Siemens Phenom
Siemens Phenom

Refer the attached SNAP document, "Chapter 2: Using the NX Journal Editor" has examples.

 

Source: NX 10 Documentation

https://docs.plm.automation.siemens.com/tdoc/nx/10/nx_api/#uid:index_snap_ref_guide