Cancel
Showing results for 
Search instead for 
Did you mean: 

Large pattern of a hole?

Creator
Creator

I am trying to create a part with a large array of honeycomb cells on the order of 100-200 (so not a ridiculous amount like several thousand). Currently, the part is made by extruding a block, and subtracting away 2 of the honeycombs, and then using pattern face to replicate the honeycomb. However, it still takes almost 10 minutes or so to process everytime the part is built. Is there a faster way to replicate this feature or is pattern face my best bet?

13 REPLIES 13

Re: Large pattern of a hole?

Honored Contributor
Honored Contributor

Pattern face will be faster than pattern feature, so I have no suggestions. 

 

As an experiment a few weeks ago, I did a pattern face on about 1200 hex holes, and it too minutes (probably in your 10 range), and then tried it with pattern feature, which I ended up killing the process after 90 minutes or so.

-Dave
NX1867(if it had versions) | Teamcenter 11.6 | Windows 10

Re: Large pattern of a hole?

Creator
Creator
I figured as much. Even trying to "pattern geometry" at the sketch level is taxing.

Re: Large pattern of a hole?

Siemens Esteemed Contributor Siemens Esteemed Contributor
Siemens Esteemed Contributor

@rbuntu wrote:
I figured as much. Even trying to "pattern geometry" at the sketch level is taxing.

That's odd...  I'm finding that pattern inside the Sketch Task Environment, or Pattern Geometry and selecting a sketch is far quicker that using Pattern Face on the extrusion faces.

Re: Large pattern of a hole?

Creator
Creator
It seems to be quicker to create the curves, but then the actual extrusion seems to take just as long.

Re: Large pattern of a hole?

Siemens Esteemed Contributor Siemens Esteemed Contributor
Siemens Esteemed Contributor

Here's my mini benchmark for comparison:

 

# of Honeycomb Holes Time to Extrude (seconds)
56 5
224 20
504 40
896 125
1400 350

 

NX 10 part attached - change the value of p1 (in multiples of 100).

Re: Large pattern of a hole?

Solution Partner Creator Solution Partner Creator
Solution Partner Creator

Hello,

the way I did tasks like that is with a positive body of the hole (internal boolean operation set to "none") in combaination with pattern geometry. As the last step I create a feature group and one subtract at the end.

 

Another possibility is to create a point set and select the feature while creating the holes. In a short test it was also very fast.

 

You can try this out.

 

Best regards,

Christian

Re: Large pattern of a hole?

Valued Contributor
Valued Contributor

Correct!

It is so much better to think of the cut as a positive geometry, pattern it, pack it in a feature group, cut it using the Selection Intent "Bodies in Group", chose the feature group and boom, done!

Re: Large pattern of a hole?

Creator
Creator

 Thanks for this, although mine is slightly different becasue there are fillets at the edges of each honeycomb.

Re: Large pattern of a hole?

Creator
Creator
I will try this and get back to you