Cancel
Showing results for 
Search instead for 
Did you mean: 
Highlighted

Legacy Mating Conditions Vs Assembly Constraints

Siemens Phenom Siemens Phenom
Siemens Phenom

Need some expertise comment on Legacy Mating Conditions Vs Assembly Constraints

 

While exploring about assembly constraints, I read words "Leagcy Mating Conditions"

 

Is this the older term used for assembly constraints that we refer in current NX versions.

 

Can somebody elaborate if there is any other difference between mating conditions and assembly constraints? 

Regards,
Ganesh
#IngenuityIsNX | NX - What's New

4 REPLIES

Re: Legacy Mating Conditions Vs Assembly Constraints

Phenom
Phenom

Hello Ganesh_Kadole,
historically assembly constraint were introduced with NX5 and have cohabited with the mating condition up to version NX7.

Since version NX7.5 there are only assembly constraint.
The differences between the two methods are many, the main one, in my opinion, is that the mating condition are

unidirectional.
This involved a different way of building assemblies: for example consider the Part A connected by the mating condition with the Part B, if you used the command move component you could just move only the Part B, while the part A is moved with the Part B while maintaining the constraints.
There are many other differences also in the visualization and management but would require an entire book .... I hope I explained.
Ciao Cesare

Re: Legacy Mating Conditions Vs Assembly Constraints

Legend
Legend

Anyone know how to delete these old "Legacy Mating Conditions?"

 

I need to move some components and they are all stuck together. I see no way to remove the relationships between them. 

Glenn Balon
Production: NX 12.0.2 MP5 Primarily CAM

Re: Legacy Mating Conditions Vs Assembly Constraints

Phenom
Phenom

Ciao @TechniCsNC ,

 

use the Convert Mating Conditions command

 

convert.png

Re: Legacy Mating Conditions Vs Assembly Constraints

Siemens Phenom Siemens Phenom
Siemens Phenom

Hi @TechniCsNC ,

Individual mating conditions can not be deleted. As @Cesare suggested, convert them to assembly constraints which can be suppressed/deleted.

Regards,
Ganesh
#IngenuityIsNX | NX - What's New