Cancel
Showing results for 
Search instead for 
Did you mean: 

License Feature - where to find the function in NX

Builder
Builder

Hello,

 

I have find in my license-file these Features:

nx_spsd_stress

nx_spsd_vibration

ug_nas_des

nx_nas_bn_basic_dsk

nx_nastran_export

ug_prod_des_advisor

 

Where can I find the related function in NX? Do I have to install additional software - other than NX?

 

Michael

Michael Eichelberg, CAD-Consultant, Dr. Wallner Engineering Nord GmbH
Production: NX10.0.3 MP16, NX11.0.1 MP4
Development: Batch and VB Testing: NX12
4 REPLIES

Re: License Feature - where to find the function in NX

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

When you use the typical installation, everything that you listed is installed.

The licenses resemble the stress and vibration wizards and NX simulation, aka Nastran.

Stefan Pendl, Systemmanager CAx, HAIDLMAIR GmbH
Production: NX10.0.3, VERICUT 8.2, FBM, MRL 3.1.7 | TcUA 10.1 MP7 Patch 0 (10.1.7.0) | TcVis 11.4
Development: C (ITK), .NET, Tcl/Tk Testing: NX12.0 | AWC 3.4 Preparing: NX12.0

Employees of the customers, together we are strong Smiley Wink
How to Get the Most from Your Signature in the Community
NX Customization - Best Practice Guide

Re: License Feature - where to find the function in NX

Builder
Builder

Yes I know it. I have installed everything. But I want to know where in NX are the funktion or where is the button in Ribbon or Menu.

 

Michael

Michael Eichelberg, CAD-Consultant, Dr. Wallner Engineering Nord GmbH
Production: NX10.0.3 MP16, NX11.0.1 MP4
Development: Batch and VB Testing: NX12

Re: License Feature - where to find the function in NX

Siemens Phenom Siemens Phenom
Siemens Phenom

Hi Michael,

 

unfortunately there is no function for it. The only way to find out is to try the function and look into the license log file on the license server to find which license bit was used.

But even this is also not always 100% true. For example, if you create a wave link and you have the Wave control license, you'll get an option to create a position-independent link. If no Wave control license is available, you don't get this option. No indication in the license log for that one....

 

And a short addition to Stefan's answer: Stress and Vibration Wizard is correct and ug_prod_des_advisor today is known as "Molded Part Validation" (formerly: Product Design Advisor"). Use the command finder to locate it.

 

Sorry no better answer.

Johannes

Re: License Feature - where to find the function in NX

Siemens Phenom Siemens Phenom
Siemens Phenom

And just so everyone knows, the wizards appear on a resource bar called process studio.

 

Wizards.png

 

In addition there is video done by John Baker showing the stress wizard in the Knowledge Base. It can be found here:

 

CAE Stress Wizard - Knowledge Base

 

Scott