Cancel
Showing results for 
Search instead for 
Did you mean: 

License error 10097

Solution Partner Valued Contributor Solution Partner Valued Contributor
Solution Partner Valued Contributor

Hello,

I have a problem with license in NX12.

I was looking for something about this bug on the forum and I found it was the fault of the license server version. Unfortunately, I currently have the latest version 8.2.5. The generated log from lmtools shows that there is a problem with hostid:

 

[...]

Licenses are case sensitive for ugslmd
14:33:34 (ugslmd)
14:33:34 (ugslmd) Wrong hostid on SERVER line for license file:
14:33:34 (ugslmd) C:\Program Files\Siemens\PLMLicenseServer\CAM_12.lic
14:33:34 (ugslmd) SERVER line says COMPOSITE=2B6522895CA1, hostid is COMPOSITE=92ECF79A7467
14:33:34 (ugslmd) Invalid hostid on SERVER line
14:33:34 (ugslmd) Disabling 1 license from feature NX10450(08A9 465D 27E3 C01D )

[...]

 

I tried stop/start server and reread the license file, but everything is ok.

In the license file, I have the name of my computer as the server name. Does anyone know what the problem is?

========================================
Engineering >> NX10.0 Performance in the making
4 REPLIES

Re: License error 10097

Siemens Phenom Siemens Phenom
Siemens Phenom

Did you replace latest license file?

Regards,
Ganesh
#IngenuityIsNX | NX - What's New

Re: License error 10097

Legend
Legend


Hi

According to your log file, Your License file do not issued for current Server PC.
COMPOSITE ID (CID) is unique value for Server Hardware.

If you change some of Hardware of your Server such as Ethernet card or a Wireless card,

the CID can be changed.

Try to contact your maintenance vender for new license file.


 Sunkap Ahn, Senior Support Engineer


logo

Re: License error 10097

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

And in case you are wondering, to get the CID run the program:

 %UGII_BASE_DIR%\UGFLEXLM\getcid.exe

 

This program is also available in the install files (DVD or ZIP) and on the GTAC download site.

Ken Akerboom Sr CAx Systems Engr, Moog, Inc.
Production: NX10.0.3.5 MP16/TC11.2
I'd rather be e-steamed than e-diseaseled


Re: License error 10097

Solution Partner Valued Contributor Solution Partner Valued Contributor
Solution Partner Valued Contributor

Thanks for help, problem solved Smiley Very Happy

========================================
Engineering >> NX10.0 Performance in the making