Cancel
Showing results for 
Search instead for 
Did you mean: 

Licenses used

Honored Contributor
Honored Contributor

If I wanted to monitor which specific licenses in our bundles, a particular user checkd out during a typical day, what would be the best way?  Is there a local log? or would I have to pick thru a server log of everyone?

 

Basically, I want to see what the typical designer uses, so we can evaluate which ones we need, and which ones we don't need.  I have the License Status tool, which helps, but that seems to only capture a moment in time.

 

Thanks!

-Dave
NX1867(if it had versions) | Teamcenter 11.6 | Windows 10
7 REPLIES 7

Re: Licenses used

Phenom
Phenom

Re: Licenses used

Honored Contributor
Honored Contributor

Those seem geared more towards monitoring a server, ratherthan a user, but I will keep digging.

 

I've been using this https://charleswb.github.io/LicenseStatus/ and it just involved manual filtering, and taking snapshots thruout the day.

-Dave
NX1867(if it had versions) | Teamcenter 11.6 | Windows 10

Re: Licenses used

Phenom
Phenom

for what is worth, I'm also attaching a picture of the (free) tool we have for this.

You pick the specific license in a bundle and you can see the relevant usage

(I think the users issue can be addressed as well)

 

As you say you want to evaluate which licenses you need, well, this is not going

to help much as specific licenses cannot be usually bought individually

 

flex1.png

 

Re: Licenses used

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

There is a log file on the license server.

I typically open a command prompt window

use "findstr" command on the username:

findstr /i username ugslmd.log

 

If you want to filter out denials, you can:

findstr /i username ugslmd.log | findstr /v DENIED

 

Change "username" & log file name as needed for your situation

Ken Akerboom Sr CAx Systems Engr, Moog, Inc.
Production: NX10.0.3.5 MP16/TC11.2
I'd rather be e-steamed than e-diseaseled


Re: Licenses used

Phenom
Phenom
the problem I have found with the log is that is never complete, due to the frequent maintenance resets of the license server deleting it.
Whenever I needed to search it for some data I have never been able to find what I wanted.
Storing the usage data in a database fixes this problem, but that requires some extra work, of course.

Re: Licenses used

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

Have IT use a .BAT to restart the license server.

I leave it as an exercise to the reader to get the current date/time & format it for the "rename" ;-)

 

NET STOP ...

REN ugslmd.log ugslmd.log_date

NET START...

Ken Akerboom Sr CAx Systems Engr, Moog, Inc.
Production: NX10.0.3.5 MP16/TC11.2
I'd rather be e-steamed than e-diseaseled


Re: Licenses used

Phenom
Phenom
that's a good idea Ken, I will have a go