Cancel
Showing results for 
Search instead for 
Did you mean: 

Limit clients on license server with physical mac addresses

Pioneer
Pioneer

We have a server with 60 floating licenses and we want to define the client PC's with their composite ID's on server so that only these computers can get license and launch NX11.0.2.

 

Is this possible? Which part of the license file on server should we edit?

 

14 REPLIES

Re: Limit clients on license server with composite IDs

Solution Partner Phenom Solution Partner Phenom
Solution Partner Phenom

You can't limit clients via the license file.

If you have 'node locked' bundles (as opposed to 'floating' ones) then they will already be locked to either a dongle or a MAC address, limiting the usage to the specific dongle or computer with the MAC address.

 

If you have floating bundles, then you are able to limit their usage by using an options file.

 

There is a document in GTAC which covers this: Using a license options file

Anthony Galante, Senior Support Engineer
PhoenxPLM
24 versions of NX installed: NX4 to NX12, plus TC11.2

Re: Limit clients on license server with composite IDs

Esteemed Contributor
Esteemed Contributor

Note in the install files (DVD from Siemens, or ZIP you download from their web server) there is a documentation folder, which has a PDF describing all the OPT file options as well.

I'm at home now, so I don't have it readily available to tell you the exact filename.

Ken Akerboom Sr CAx Systems Engr, Moog, Inc.
Production: NX10.0.3.5 MP16/TC11.2
I'd rather be e-steamed than e-diseaseled


Re: Limit clients on license server with composite IDs

Pioneer
Pioneer
Ok thanks for the tip, we have managed to create an opt file and included computers with their hostnames. The server runs OK now.

As far as I’ve seen in describing pdf, we can only define computers with username, hostname or IP. There is no Mac adress option I guess. Is this correct? Because hostname of a pc is not unique and this may lead misuse.
Any ideas?

Re: Limit clients on license server with composite IDs

Esteemed Contributor
Esteemed Contributor

You can use IP address ranges or specific IP addresses.

 

HOST_GROUP ABC  001.002.*.* 002.003.*.*
INCLUDE NX10105 HOST_GROUP ABC

Juts be aware of DHCP changing addresses for whatever reason

 

Ken Akerboom Sr CAx Systems Engr, Moog, Inc.
Production: NX10.0.3.5 MP16/TC11.2
I'd rather be e-steamed than e-diseaseled


Re: Limit clients on license server with composite IDs

Pioneer
Pioneer
How about mac adresses (for example 12:ab:34:56:c7)

Re: Limit clients on license server with physical mac addresses

Siemens Phenom Siemens Phenom
Siemens Phenom

I just go by user names. Makes management a whole lot easier because users upgrade and change computers over time but their user names do not change.


Larry Carpenter, P.E.
CAxPLM Architect @ Siemens Molecular Imaging
Past Board Member @ PLM World, Inc,

Re: Limit clients on license server with physical mac addresses

Pioneer
Pioneer
Yeah but there will be like 2000 students and we don’t want unauthorized ones to use NX.

Re: Limit clients on license server with physical mac addresses

Esteemed Contributor
Esteemed Contributor

Then I suggest you hire a student ;-) to write a bit of code to create the OPT file "on-the-fly" from a list of usernames.

Can you get the user info from class registrations (or whatever) to automate getting the list of users?

If so, then the utility could just be re-run if students add/drop the class (during the semester)

 

Note you'll also have to allow the professors/TAs/whomever needs "permanent" access, but isn't registering for one of the classes...

 

If you don't automate this, it will be a PITA.

 

Would the users be using their own PCs to run NX, or only PCs in a designated "lab"?

If the latter, would the IT group support setting them up with a unique IP address range to allow filtering based on IP (or do other users, who should not have access to NX, use the same PCs?)

Ken Akerboom Sr CAx Systems Engr, Moog, Inc.
Production: NX10.0.3.5 MP16/TC11.2
I'd rather be e-steamed than e-diseaseled


Re: Limit clients on license server with physical mac addresses

Esteemed Contributor
Esteemed Contributor

Note the user names do NOT all need to be on the same line, e.g. something like this should work:

 

GROUP NX_USERS asmith
GROUP NX_USERS bsmith
GROUP NX_USERS csmith
GROUP NX_USERS dsmith

INCLUDEALL GROUP NX_USERS 

Might make it easier to automate...

 

Ken Akerboom Sr CAx Systems Engr, Moog, Inc.
Production: NX10.0.3.5 MP16/TC11.2
I'd rather be e-steamed than e-diseaseled