Cancel
Showing results for 
Search instead for 
Did you mean: 

Lip / Groove Feature in NX, similar to SolidWorks Feature

Creator
Creator

Is there or are there plans to create a feature for creating a lip + groove fastening feature between two parts in NX? similar to the feature that SoldWorks has?

2 REPLIES

Re: Lip / Groove Feature in NX, similar to SolidWorks Feature

Siemens Phenom Siemens Phenom
Siemens Phenom

Hi,

Sorry i might be wrong but i don't think if we have any OOTB feature for the lip creating (for both the mating components) but as an option you can use REUSABLE features or UDF for the same. Infact you can have a library of the same.

There are lot of mold part detailing features already in the REUSABL;E OBJECT LIBRARY.(snap locks etc.).

For the lip you can optionally create a 2-D sketch and use that for the sweep (for creating the lip).

Best Regards

Kapil

Re: Lip / Groove Feature in NX, similar to SolidWorks Feature

Creator
Creator

Thanks Kapil