Cancel
Showing results for 
Search instead for 
Did you mean: 

Load case Error - Topology Opt

Pioneer
Pioneer

Hi all,

 

I started two Optimizations with quite the same components (little different)

One Optimization works well, with good results.

the other one gives always this error: " Warning: Load case(s) 1 have no loads. They will have no effect." and it quits the simulation. "Error: Simulation failed."

 

I used the same setups, also the loads are the same... I can not find the error.

 

what could it also be? like a a defective body, or ... ??

I have no idea=(

 

did anyone had a problem like that?

 

 

regards,

L

2 REPLIES 2

Re: Load case Error - Topology Opt

Siemens Phenom Siemens Phenom
Siemens Phenom
Hello @BachmannL,

Just from the top of my head, the bodies that are not included in the design space, leave them out, rather then adding them and use the option "out".

I might need to check te menu to get the wording correct Smiley Happy

Kind regards,

Dennis
Dennis de Brouwer
Application Support Engineer
GTAC EMEA - Siemens Industry Software

Re: Load case Error - Topology Opt

Pioneer
Pioneer
Now it works, maybe it was to less material in the designspace for the force we needed...Smiley Wink