Cancel
Showing results for 
Search instead for 
Did you mean: 
Highlighted

MULTIPLE SHEETS AND AFTER PRINTING ALL SHEETS HAS TO COME IN ONE PDF FILE

Solution Partner Valued Contributor Solution Partner Valued Contributor
Solution Partner Valued Contributor

Hello all,

 

lets say I have 5 sheets in drafting and after printing i need all the sheet pdfs into single as we do like merge sheets kind of thing..

 

 

Is it possible...!!!

 

 

 

2 REPLIES 2

Re: MULTIPLE SHEETS AND AFTER PRINTING ALL SHEETS HAS TO COME IN ONE PDF FILE

Phenom
Phenom

@karthik6

in the PDF export dialogue window you can pick several sheets when you hold CTRL during selection.

All the chosen drafts will be in the PDF.

 

2018-03-28_09.pngNX11 Export PDF dialog

 

Below the save path you can also check "append".

This will then add these drawings to an existing PDF if wanted.

Huysmans Metalen n.v.
2x NX 12.0.2.9 Mach Designer
on Win10 64bit
NX Beta Tester with focus on Sheet Metal
Command Finder is your friend

Re: MULTIPLE SHEETS AND AFTER PRINTING ALL SHEETS HAS TO COME IN ONE PDF FILE

Solution Partner Valued Contributor Solution Partner Valued Contributor
Solution Partner Valued Contributor

Thank you @frank_nx Smiley Happy