Cancel
Showing results for 
Search instead for 
Did you mean: 

MUTLIPLE STEP FILES OPEN IN A SINGLE STEP FILE

Solution Partner Valued Contributor Solution Partner Valued Contributor
Solution Partner Valued Contributor
Hello all,

One of my client whenever he tries to open a step file after importing it comes along with an another step or iges file gets opend along with that so they've reinstalled NX and it was working fine, again after a few months he started getting this issue.
Can anyone suggest me only reinstallation is we have to do even though I guess it's not a std solution or any other methods to resolve this!

Thanks in advance
2 REPLIES

Re: MUTLIPLE STEP FILES OPEN IN A SINGLE STEP FILE

Legend
Legend

Hi.

If you mean, when he import STEP file by opening .stp file, another body is created beside bodies from current STEP file.

At first, open step log file, and then you can check number of imported bodies.
ex) ! INFO- Total number of solids input for this translation : 1

If it is not same with bodies of result part file,
the step seed part maybe including existing bodies already. (although almost impossible)

Open and check .prt files in [%ugii_base_dir%\STEP203UG (or \STEP214UG)].
ex) step203ugnullnx100_mm.prt

 Sunkap Ahn, Senior Support Engineer


logo

Re: MUTLIPLE STEP FILES OPEN IN A SINGLE STEP FILE

Solution Partner Valued Contributor Solution Partner Valued Contributor
Solution Partner Valued Contributor
Sure I will take a look into that Smiley Happy


Thank you