Cancel
Showing results for 
Search instead for 
Did you mean: 

Made a new section in assembly why not visible in drafting ?

Genius
Genius

Hello

I made a new section in assembly. Why sections are not visible in drafting ?

  • Creating a base view and no "section" model views available ?
  • It shows up in assembly as a section though ?

What are these assembly sections ?

If they do not show up in drafting ?

2 REPLIES 2

Re: Made a new section in assembly why not visible in drafting ?

Siemens Phenom Siemens Phenom
Siemens Phenom

Are you using Edit Section/Clip Section command to create section of assembly in UI?

 

Use 'Create Section View' or 'Create Lightweight Section View' command depending upon your requirement.

 

If you are not aware of the difference between these two, you can refer the documentation link always.

 

https://docs.plm.automation.siemens.com/tdoc/nx/10/nx_help/#uidSmiley Tonguemi_section_views_ltwt_sectionvw_ov

 

https://docs.plm.automation.siemens.com/tdoc/nx/10/nx_help/#uidSmiley Tonguemi_menu_sectionvw_ov

 

Section.PNG

 

 

Section1.PNG

 

 

section2.PNG

 

 

Re: Made a new section in assembly why not visible in drafting ?

Solution Partner Phenom Solution Partner Phenom
Solution Partner Phenom
check the model views of the part in modeling.
all the view there are available in modeling are shown in the base view command in drafting.

So if you don't see the section views here you don't see them in drafting.

Ruud van den Brand
Pre-sales NX CAD
cards PLM Solutions