Cancel
Showing results for 
Search instead for 
Did you mean: 
Highlighted

Maintaining User Selections from List

Creator
Creator

Hi, 

 

I have been programming a GUI in which the users have the option to select components from different drop-down enumeration boxes. Based on what they select in the first block the list of options for the following boxes may change. My question is whether or not there is a way to keep the selection of the second box even if the list changes.

 

For example, if the user selects Option A from block 1 and size 3 (from a list of 1, 2, or 3) from Block 2, is there a way to keep the second block to show a selection of 3 if they go back and choose Option B from block 1? In this instance we're assuming the list of options for the second block didn't change but it could if the user had selected, say, Option C. 

 

I appreciate any help, thanks!

1 REPLY 1

Re: Maintaining User Selections from List

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

I think a better place to post this question would be in the programming and customization forum.