Cancel
Showing results for 
Search instead for 
Did you mean: 
Highlighted

Making a file read-only in NX 11?

Creator
Creator

Hi there,

 

How can I save a part file as read-only, so that other people can only access a read-only version and cannot make changes until they save-as? There is surprisingly little documentation on this.

 

Thanks!

1 REPLY 1

Re: Making a file read-only in NX 11?

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

Native or Teamcenter?

 

Native mode you deal with the operating system access control.

On Windows, you can "right click on the file" -> Properties -> Check the "read only" tab (but then it is read-only for you as well)

Or try to set up "right click on the file" -> Properties -> "Security" tab stuff.

If on a network share, you may need to talk to the admin of the network share to set something up.

 

Teamcenter - depends how Teamcenter is set up.  You could change it so only the owner of a file has write access.  You may then also have to restrict who can change ownership.  There are other ways as well (projects, etc.)  As well as manual changing "Access" settings

Ken Akerboom Sr CAx Systems Engr, Moog, Inc.
Production: NX10.0.3.5 MP16/TC11.2
I'd rather be e-steamed than e-diseaseled