Cancel
Showing results for 
Search instead for 
Did you mean: 

Material Creation by Varying some of the properties of already existed material

Valued Contributor
Valued Contributor

hi Community,

 

 in nx 9.0 i have the material library no i want to create a new material by changing some of the properties of already existed material in nx material library..but i did in one way like i copied the material from library then it is showning in local materials so from there i am able to change the properties whatever i want but after closing the file the and i am going to apply to a another file that material is not there..

1 REPLY 1

Re: Material Creation by Varying some of the properties of already existed material

Honored Contributor
Honored Contributor

As I recall, you will have to merge the new local material, with the global list.  Materila Library Manager, local materials, then select the material, and RMB and export to the correct library.

-Dave
NX 11 | Teamcenter 11 | Windows 10