Cancel
Showing results for 
Search instead for 
Did you mean: 

Max circle diameter between aero sections

Solution Partner Pioneer Solution Partner Pioneer
Solution Partner Pioneer

Hi

 

In the images below, you will see a circle that's tangent to two opposing faces of an aero section, is there a way to constrain the circle to the location that would indicate the greatest distance bewteen the two faces such that the circle is the largest possible size it could be given its tangential contraints?

 

Cheers

 

Si

circle.JPG

1 REPLY 1

Re: Max circle diameter between aero sections

Genius
Genius

Take a look at this.

 

https://community.plm.automation.siemens.com/t5/NX-Design-Forum/Wing-profile-dimensioning/td-p/48356...

 

 

Add a line through the center of your circle and use the point on curve constriant to both the circle and the wing profile.

Kurt Neubaecker
CAD/CAM Designer
Proficient Industries
Cleveland, Ohio