Cancel
Showing results for 
Search instead for 
Did you mean: 

Measure Load Time

Creator
Creator

Is there a tool to measure load time, show cachesize/ram use from assemblies, parts etc.?

8 REPLIES 8

Re: Measure Load Time

Siemens Phenom Siemens Phenom
Siemens Phenom

Hi,

You can try the NX log file ..HELP/LOG FILE

It will give you some statistics you want.

Best Regards

Kapil

Re: Measure Load Time

Siemens Experimenter Siemens Experimenter
Siemens Experimenter

You can measure it using stop watch. We usually measure this using stop watch only.

Re: Measure Load Time

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

If you need repeatable tests,  you could use journals to log the times.

Probably a lot more reliable than stop watches (I usually get distracted at just the wrong moment :-)

Ken Akerboom Sr CAx Systems Engr, Moog, Inc.
Production: NX10.0.3.5 MP16/TC11.2
I'd rather be e-steamed than e-diseaseled


Re: Measure Load Time

Siemens Experimenter Siemens Experimenter
Siemens Experimenter

Check syslog, you will get the data of load.

Re: Measure Load Time

Creator
Creator

 

How do I run NX with cmd? Should I create e new entry in system environment variables "TIME_USER_EVENTS=1"?

Re: Measure Load Time


@inmediasp wrote:

 

How do I run NX with cmd? Should I create e new entry in system environment variables "TIME_USER_EVENTS=1"?


This variable needs to be defined before NX starts - there is no requirement to run with CMD. It is set the same as any other variable - in your ugii_end.dat file, or your .bat file, or in your system environment variables, or ...

Mark Rief
Retired Siemens

Betreff: Measure Load Time

Creator
Creator

Syslog is to messy, too much information at once. Is there maybe a better solution to show load time of assemblies/parts via nx open?

Betreff: Measure Load Time

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

Note you can write your own text to the syslog (UF_print_syslog).

If you include "unique" text (e.g. "KEN IS STARTING TO OPEN FILE XYZ at 10:32 AM",  "KEN IS DONE OPENING ...")

 

You can then use "findstr" to parse the syslog for "KEN"

 

Or you could write to the "information" window  (UF_UI_open_listing_window, UF_UI_write_listing_window) if that makes more sense to you.

 

Ken

Ken Akerboom Sr CAx Systems Engr, Moog, Inc.
Production: NX10.0.3.5 MP16/TC11.2
I'd rather be e-steamed than e-diseaseled