Cancel
Showing results for 
Search instead for 
Did you mean: 

Measure point

Creator
Creator

How to measure point in NX 8.5 ?

5 REPLIES 5

Re: Measure point

Siemens Phenom Siemens Phenom
Siemens Phenom

Use 'Measure Point' command (Menu > Analysis > Measure Point). Associative measurement can be created with individual coordinate expresssions which can be used later in the modeling/drafting if needed. 

 

https://docs.plm.automation.siemens.com/tdoc/nx/10/nx_help/#uid:index_measure_enter_values:xid600601

 

 

Re: Measure point

Creator
Creator

hi

 

In NX 10 am getting that option..but in NX 8.5 am not able to find that one

Re: Measure point

Siemens Phenom Siemens Phenom
Siemens Phenom

Use command finder to locate/start the command.

Re: Measure point

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

If I remember correctly, "measure point" was introduced in NX 9. In versions prior to NX 9 you can use the command information -> point to query the point's coordinates, but there is no option to save them as expressions.

Re: Measure point

Siemens Phenom Siemens Phenom
Siemens Phenom

Oh! I was not aware of that. Smiley Tongue 

@Raki: Give try for 'Coordinate Note' command from PMI application.