Cancel
Showing results for 
Search instead for 
Did you mean: 

Modal frequency response

Experimenter
Experimenter

Hi everyone,

I am new on this platform and new to NX 11. I am trying to perform Modal frequency response analysis for a very simple stator geometry. I have done the modal anlaysis successfully and i know the natural frequencies. What i am left with is performing the modal frequency analysis response. How do I set up the frequency response analysis and apply the following frequency-dependent loads to the stator teeth?

Let say these are the loads: 

843Pa--66.66Hz

100Pa--133.33hz

443Pa--200hz.

Thank you very much and look forward to your suggestions.

 

1 REPLY

Re: Modal frequency response

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

Hi there @Malema,

 

I think you would be better served, posting this in the NX-Design Forum....link below.

 

https://community.plm.automation.siemens.com/t5/NX-Design-Forum/bd-p/NXDesignForum

Sean Cresswell
Design Manager Streetscape Ltd
Solid Edge 2019 [MP4] Classic [x3 Seats - Cloud Enabled]
Windows 10 - Quadro P2000