Cancel
Showing results for 
Search instead for 
Did you mean: 

Model view or Drafting view

Honored Contributor
Honored Contributor

In the master model world...

 

Is there a way to tell where the view came from, model file or drawing file?  User created an explosion in the drawing file, and added it to the drawing.  Now it's not exploded.  I can re-add the exploded view fine, so I'm wondering if they created a view from the model file, instead of the drawing file.

 

I've been looking at properties, and anything I can think of, but nothing has tipped me off yet.

-Dave
NX 11 | Teamcenter 11 | Windows 10
1 REPLY 1

Re: Model view or Drafting view

Siemens Phenom Siemens Phenom
Siemens Phenom

Yes - Use the Menu->Information->Object command and then select the view on the drawing. In the information window, the name of the part associated with the view will be displayed under the "Drawing Member View Display Settings" section.