Cancel
Showing results for 
Search instead for 
Did you mean: 

Model views give only Flat-Pattern ?

Genius
Genius

Hello

I have a 2(two) files

  1. Is the part file
  2. Is the drawing file .dwg
  • When I try to insert a regular base view of the part it only gives the Flat-Pattern ? (rotated in many ways see photo 2)
  • Is the file corrupted what can I do ?

 

Flat-pattern bug.png

 

flatpatimany.png

3 REPLIES 3

Re: Model views give only Flat-Pattern ?

Siemens Phenom Siemens Phenom
Siemens Phenom

Can you please share the sample part file, so that it would be helpful to have clear understanding of this problem. 

Re: Model views give only Flat-Pattern ?

Solution Partner Phenom Solution Partner Phenom
Solution Partner Phenom
Did you check all your model views in modeling?
how are the showing when you open the .prt file in the modeling application?
if you double click the model view is it then also showing the flatt pattern?

Ruud van den Brand
Pre-sales NX CAD
cards PLM Solutions

Re: Model views give only Flat-Pattern ?

Phenom
Phenom

It almost looks like you're trying to insert a "projected view" from a "flat pattern view" and then you will also see things like you're showing.

I just checked that in NX10, and that's not even possible anymore; Flat Pattern Views cannot be selected for creating a projected view.  But maybe you still could in NX9.

 

Huysmans Metalen n.v.
2x NX 12.0.2.9 Mach Designer
on Win10 64bit
NX Beta Tester with focus on Sheet Metal
Command Finder is your friend