Cancel
Showing results for 
Search instead for 
Did you mean: 

Modeler Error!!!!!

Hi ,

 

Did someone faced this issue!!!! Modeler/Kernel has not been interrupted.

I have been working in NX11 model and due to this error I can't edit/rollback features(May be corrupted). I have no idea how to fix this problem!!!!!

Picture attached.

 

Thanks,

Devaraj.

7 REPLIES

Re: Modeler Error!!!!!

Siemens Phenom Siemens Phenom
Siemens Phenom

No option or setting to control this kind of error. Open IR with GTAC.

Regards,
Ganesh
#IngenuityIsNX | NX - What's New

Re: Modeler Error!!!!!

Siemens Phenom Siemens Phenom
Siemens Phenom

Probably best to log with GTAC helpdesk

 

Steve V

Re: Modeler Error!!!!!

Siemens Honored Contributor Siemens Honored Contributor
Siemens Honored Contributor

Similar issue reported in PR 7862665, which was fixed in NX11.0.1.  Which version of NX11 do you have installed? 

 

Regards, Ben

Re: Modeler Error!!!!!

Hi Ben,

Version-NX 11.0.0.33

Thanks

Re: Modeler Error!!!!!

Phenom
Phenom
Usually best to install the maintenance packs/releases if you can, rather than sticking to the very first release, as that typically fixes bugs of this nature. In fact, most seasoned users would recommend waiting on the first MR/MP before jumping to a new version, if at all possible.
-Tim

Re: Modeler Error!!!!!

Siemens Honored Contributor Siemens Honored Contributor
Siemens Honored Contributor

Hi @Devraj_Mendon,

 

Version-NX 11.0.0.33

As you probably know, that is the base release of NX 11.  In order to take advantage of the fix that was delivered with PR 7862665, you will need to install Maintenance Release (MR) NX 11.0.1 to see if the fix corrects the issue you reported.  You can download MR's here

 

Regards, Ben

Re: Modeler Error!!!!!

Thank you for your suggestions.