Cancel
Showing results for 
Search instead for 
Did you mean: 

Modeling Text default

Gears Phenom Gears Phenom
Gears Phenom

In NX 9, is it possible to set a default font, for the modeling text?  (Modeling -> Curve, Text)  or do I have to set it in the model seed file?

 

TextDefault.jpg

-Dave
NX 11 | Teamcenter 11 | Windows 8.1
3 REPLIES

Re: Modeling Text default

Genius
Genius
I think it is saved in the dialog memory, isn't it?

Re: Modeling Text default

Gears Phenom Gears Phenom
Gears Phenom

It is.  I was hoping for a default setting, so we don't have to rely on the user changing it at all.

 

Thanks!

-Dave
NX 11 | Teamcenter 11 | Windows 8.1

Re: Modeling Text default

Siemens Phenom Siemens Phenom
Siemens Phenom
Existing ER 2080126

Regards, Ben