Cancel
Showing results for 
Search instead for 
Did you mean: 

Modeling of a ball endmill

Creator
Creator

I have to accurately model a ball endmill with spiral flutes and the correct primary and secondary cutting edges. Does anybody know of some NX wizard or program that can generate this? 

Thanks, Steve

5 REPLIES 5

Re: Modeling of a ball endmill

Creator
Creator

Well, 156 views in a week and no replies. I guess that answers the question. Smells like an opportunity!!!! 

Re: Modeling of a ball endmill

Genius
Genius

ball end mill ... interesting shape ...

 

Page 144 4 Flute SE Ball Reg.jpg

Re: Modeling of a ball endmill

Legend
Legend

There are some on Grabcad

Rob Newcomb, CAD/CNC/Simulation manager
Elmhirst Industries, Specializing in Prototype sheet metal stampings and assemblies

Production: NX 12.0.2 / Autoform r8 /WorkNC 2019 r1
Testing:NX 1855
PC: Rave Cadbeast: Intel(R) i7-4790K CPU @ 4.GHz /32gb ram /NVIDIA Quadro P2000 on Win10 Pro

Re: Modeling of a ball endmill

Phenom
Phenom
I don't think you will find any specific function inside of NX for the creation of the type of geometry.
But you should really look at Swept Solid function.

Re: Modeling of a ball endmill

Pioneer
Pioneer
NX 11 provide option to sweep solid .. Hope this will help