Cancel
Showing results for 
Search instead for 
Did you mean: 

Modeling using Points- update

Pioneer
Pioneer

Hello All

 

I need to create a aerofoil profile using the set of points given.
(Say 89 points for one cross section, and it has 5 sections for aero geometry).

 

The tag is these points might get changed in future. So need to create the profile in such a way, in case of future update / Deletion of any existing point / addition of more points, the modeled profile should get updated accordingly.

 

I have dat files for all five sections (5 files), which is the input file for geometry.

 

Can any one suggest me a best possible solution ?

 

/Sathyaraj

NX 9.0 / TC 10.0

3 REPLIES 3
Highlighted

Re: Modeling using Points- update

Siemens Phenom Siemens Phenom
Siemens Phenom

Hi ,

you can consider Knowledge Fusion as one of your option.

Regards

Kapil

Re: Modeling using Points- update

Siemens Phenom Siemens Phenom
Siemens Phenom

You can create a series of 'Point Set' group from the data files and then create a Spline by selecting one of these point set groups.  Later if the data changes you can create a new 'Point Set' group and then edit the existing curve by replacing the original point set with the new one and everything will update as expected.

John R. Baker, P.E. (ret)
EX-Product 'Evangelist'
Irvine, CA

Re: Modeling using Points- update

Experimenter
Experimenter

Any chance of elaborating, John? Which spline creation method?