Cancel
Showing results for 
Search instead for 
Did you mean: 

Modified component visibility in assembly, Reference sets

Valued Contributor
Valued Contributor

When working in assemblies, I typically have the components set to a reference set of "Solid" so that I can have the datums and other construction geometry hidden. (The Solid reference set I created just includes the solid features of the part.)  If I want to modify a feature in one of the component parts, I have to change the reference set of that component to Entire Part; otherwise the internal sketch of that feature will not be visible. 

 

Is there a setting or something that can be changed so that the internal sketch (not external) is visible for feature modification when I have the part set to a reference set of Solid?  I basically don't want to have to switch reference sets of a component before I modify the part.  Thanks

1 REPLY

Re: Modified component visibility in assembly, Reference sets

Gears Phenom Gears Phenom
Gears Phenom

In the Customer Defaults, Assemblies, General, Work part tab, try toggling on "Display using 'entire Part' Reference Set.

-Dave
NX 11 | Teamcenter 11 | Windows 8.1