Cancel
Showing results for 
Search instead for 
Did you mean: 

Modifiying SolidWorks file in NX8.5

Experimenter
Experimenter

Hi there,

 

I am new using NX, and I have a piece created in Solid works which I need to modify. I think it is really simple, but I can't find the right tools to do it. any suggestions?

 

I am attaching the front view of my piece (1mm thickness):

 

This is how it looks...

 

FrontOld.png

 

and I would like to trim or extrude those indent "ears" to make it a circle like this:

 

FrontNew.png

1 REPLY 1

Re: Modifiying SolidWorks file in NX8.5

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

In NX, use the "delete face" command to eliminate the "ears"; select the cylindrical ear surfaces. Make sure the "heal" option is turned on.