Cancel
Showing results for 
Search instead for 
Did you mean: 

Monochrome-mode in drawing ?

Valued Contributor
Valued Contributor

What is the monochrome-mode in drawing ?

  • In default I have this horrible "dark gray+blue"-theme.
  • So if I select this monochrome selection what happens ? Does it change the files somehow ? What harm it causes if any ?
  • Monochrome looks a lot better...but are there any concerns that I must think about ?

monochrome.jpg

4 REPLIES

Re: Monochrome-mode in drawing ?

Legend
Legend

If you want color in your drawings, you may want to switch back and forth to make sure things are displayed correctly when you plot them.

 

I added a button to quickly switch back and forth between the 2. Though personally I mute all of my backgrounds to grey in the software and dull them with the monitors. bright white hurts my eyes after awhile

Rob Newcomb, CAD/CNC/Simulation manager
Elmhirst Industries, Specializing in Prototype sheet metal stampings and assemblies

Production: NX 11.0.2.7 / Autoform r7 /WorkNC 2017 r2
Testing:NX12 EAP
PC: Rave Cadbeast: Intel(R) i7-4790K CPU @ 4.GHz /32gb ram /NVIDIA Quadro K2200 on Win10 Pro

Re: Monochrome-mode in drawing ?

Legend
Legend

I like a black background.   But, I use monochrome when using the track drawing changes "overlay" command.  This way I can really see the differences in the two drawings.

Re: Monochrome-mode in drawing ?

Honored Contributor
Honored Contributor

"So if I select this monochrome selection what happens ? Does it change the files somehow ? What harm it causes if any?"

 

You can turn the monochrome option on/off at will, it will not harm your file in any way. It is only a display option. It may mark the file as "modified" because you have changed a display option, but the underlying object colors are retained. Your drawing may plot differently if you use the "colors: as displayed" option.

Re: Monochrome-mode in drawing ?

Siemens Phenom Siemens Phenom
Siemens Phenom

You can also think about it this way. The color option maybe nice for doing your detail work because you can see the different parts in your assembly. After that you turn on monochorme to see what it may look like if you do not have a color plotter. 

 

Scott