Cancel
Showing results for 
Search instead for 
Did you mean: 

Motion Simulation with Rack fixed

Pioneer
Pioneer

Dear Experts,

Is there a Rolling type of motion possible in NX? If so how?

I am looking at simulating Rack and Pinion with Rack fixed.

Thank you Verymuch.

Prasad

 

Durgavajjala S.Prasad /NX 9,NX10&NX11
6 REPLIES 6

Re: Motion Simulation with Rack fixed

Siemens Legend Siemens Legend
Siemens Legend

How about using the Rack and pinion feature ?

 

Does that help ?

 

/ Tomas

Re: Motion Simulation with Rack fixed

Pioneer
Pioneer

I tried Rack and Pinion coupler, but I am able to select either slider or revolute joints, not both.

Durgavajjala S.Prasad /NX 9,NX10&NX11

Re: Motion Simulation with Rack fixed

Pioneer
Pioneer

Please refer to attached image.

I am using a fixed rack,  a revolute (rolling) pinion and a slider support rod.

When keeping the support rod as base link for pinion, I am unable to select the created slider and revolute joints together.

(However, when base link is not selected, I am able to select both joints, but Pinion is then not rolling, just revolving.)

Please help.

Durgavajjala S.Prasad /NX 9,NX10&NX11
Highlighted

Re: Motion Simulation with Rack fixed

Siemens Legend Siemens Legend
Siemens Legend

If the model in the image, is the model, - Can you upload it ?

 

Regards,

 Tomas

Re: Motion Simulation with Rack fixed

Pioneer
Pioneer

I am uploading similar model. I am missing where to use 3D contact,coupler,... Thank you verymuch for venturing out to help.

Durgavajjala S.Prasad /NX 9,NX10&NX11

Re: Motion Simulation with Rack fixed

Pioneer
Pioneer

Finally, the '2-3 Joint Coupler' did the trick.

Durgavajjala S.Prasad /NX 9,NX10&NX11