Cancel
Showing results for 
Search instead for 
Did you mean: 

Motion simulation of multi-degree of freedom mechanism

Hello all, 

 

I have a mechanism shown in the following picture.

 

Capture.PNG

Basically, it entails a fixed spring that holds the blue rod to be in contact with 4 fixed balls. Consider one pushes the red ball at the end along the direction shown by the arrow in the picture. If the pushing force is great enough, the blue rod will rotate around the ball support on the right hand side, and will leave the contact of the left hand side ball-pair. 

 

The rotating result is similar to the following (with spring omitted).

Capture2.PNG

 

 

Since different directions of the external force acting on the grey ball will give us different motion results, due to the fact that the mechanism has multiple degrees of freedom, is it possible to simulate the mechanism?  

 

Thank you for the help.

 

Sincerely,

 

Stephen

3 REPLIES 3

Re: Motion simulation of multi-degree of freedom mechanism

Siemens Phenom Siemens Phenom
Siemens Phenom

Stephan --

 

The easy answer is yes.  :-)

 

Is this close?

 

(view in My Videos)

Taylor Anderson
NX Product Manager, Knowledge Reuse and NX Design
Tel: +1 (602) 441-0683
taylor.anderson@siemens.com

Re: Motion simulation of multi-degree of freedom mechanism

Thank you for your reply.

 

Yes, I figured that out too.

 

I would also like to know where I can find the description of functions available in the function manager? For example STEP(x,x0,h0,x1,h1), I would like to know the meaning of the variables I should put into the function.

 

Capture.PNG

 

 

Re: Motion simulation of multi-degree of freedom mechanism

Siemens Phenom Siemens Phenom
Siemens Phenom

https://docs.plm.automation.siemens.com/tdoc/nx/12/nx_help#uid:id563891

Taylor Anderson
NX Product Manager, Knowledge Reuse and NX Design
Tel: +1 (602) 441-0683
taylor.anderson@siemens.com