Cancel
Showing results for 
Search instead for 
Did you mean: 

Mouse buttons mapping

Phenom
Phenom

hello,

 

is it possible to remap mouse buttons ?

A user here would like to have MB1 + MB3 working as Pan.

It's an ordinary mouse, not a 3D pointer or other fancy device. 

AFAIK a keyboard key could be bound to Pan, but not a mouse button.

 

Tnx

 

 

4 REPLIES 4

Re: Mouse buttons mapping

Siemens Phenom Siemens Phenom
Siemens Phenom

I don't think so.

John R. Baker, P.E. (ret)
EX-Product 'Evangelist'
Irvine, CA

Re: Mouse buttons mapping

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

Only way I can think of, he could probably change the button actions at the operating system (i.e. Windows control panels) level, however this will effect ALL applications, which they may not want

Ken Akerboom Sr CAx Systems Engr, Moog, Inc.
Production: NX10.0.3.5 MP16/TC11.2
I'd rather be e-steamed than e-diseaseled


Re: Mouse buttons mapping

Siemens Phenom Siemens Phenom
Siemens Phenom

I've looked and I don't see anything there that would help.

John R. Baker, P.E. (ret)
EX-Product 'Evangelist'
Irvine, CA

Re: Mouse buttons mapping

Legend
Legend

I use a Logitech G500 "gaming" mouse.

It has a few extra programmable thumb buttons on it, I've mapped keys to those to make things easier for me.

 

I've tried Spaceballs and SpaceMice, but i'm not coordinated enough to use them effectively.

 

Rob Newcomb, CAD/CNC/Simulation manager
Elmhirst Industries, Specializing in Prototype sheet metal stampings and assemblies

Production: NX 12.0.2 / Autoform r8 /WorkNC 2019 r1
Testing:NX 1855
PC: Rave Cadbeast: Intel(R) i7-4790K CPU @ 4.GHz /32gb ram /NVIDIA Quadro P2000 on Win10 Pro