Cancel
Showing results for 
Search instead for 
Did you mean: 

Mouse buttons mapping

Experimenter
Experimenter

Is there another way to "accept" a selection other than using the middle mouse button?  I've got a bad finger and it hurts to press the mouse wheel as the middle mouse button.  I am using a 3Dconnection space ball and I'm wondering if that can be mapped.

3 REPLIES

Re: Mouse buttons mapping

Gears Phenom Gears Phenom
Gears Phenom
Doesn't help directly, but 3Dconnexion has a true 3 button cadmouse now, which I really like....but I go back to the days of 3 button mice, before the wheel.
-Dave
NX 11 | Teamcenter 11 | Windows 8.1

Re: Mouse buttons mapping

Genius
Genius

I use a 2 button SpaceNavigator from 3Dconnexion and using the 3Dconnexion Properties dialog box I set the Right button to act as the "Middle Mouse" button. So technically I'm still using the middle mouse button to accept a selection, I just defined a button on my space ball to act as the middle mouse button.

 

3Dconnexcion Button Settings.jpg

Re: Mouse buttons mapping

Valued Contributor
Valued Contributor

Get a rol free mouse with 3 buttons.

I have two mouse plugged into my laptop. One with roll wheel and one with true middle button. Ans of cause 3D Connecton's Space Mouse.

Easy as hell.