03-10-2017 12:54 AM
Hello
How to Move Face so it is exactly on the edge ?
03-10-2017 12:57 AM - edited 03-10-2017 02:34 AM
03-10-2017 03:07 AM
You can also measure the distance using DesignLogic, use the small arrow on the right of the input field.
You can set motion to "point tot point".
You can use the Replace Face command.
You can delete the face.
Use your imagination! There are so many ways to do this.
Regard,s **bleep**
03-13-2017 05:45 PM
I agree with both previous suggestions. The simplest is Replace Face. It is a geometric definition rather than finding just the right value.
03-13-2017 06:46 PM
03-13-2017 07:12 PM
Do note though that snap to object is not associtive. Replace Face or Make Coplanar are associative and have the benefit of a geometric definition rather than a value.