Cancel
Showing results for 
Search instead for 
Did you mean: 

Move view, dimensions change position

Phenom
Phenom

Hi,

when I move views dinamically, dimensions like angular and radius change their position respect the original position. Only occur to me or it's a limitation of NX 10 ?after.pngafterbefore.pngbefore

Thank you...

Using NX 11 / RuleDesigner PDM

6 REPLIES

Re: Move view, dimensions change position

Siemens Phenom Siemens Phenom
Siemens Phenom

Hi  cubalibre,

Yes i also see the same behaviour in NX10.0.3 but not in NX 9.0.3. 

I can use ORIGIN tool to fix it up though but still it is just a workaround. 

Best Regards

Kapil Sharma

Re: Move view, dimensions change position

Phenom
Phenom

@kapilsharma wrote:

Hi  cubalibre,

Yes i also see the same behaviour in NX10.0.3 but not in NX 9.0.3. 

I can use ORIGIN tool to fix it up though but still it is just a workaround. 

Best Regards

Kapil Sharma


The solution is to install NX 11.

Thank you...

Using NX 11 / RuleDesigner PDM

Re: Move view, dimensions change position

Siemens Phenom Siemens Phenom
Siemens Phenom

will do it next year certainly Smiley Happy  ....

Best Regards

Kapil

Re: Move view, dimensions change position

Valued Contributor
Valued Contributor

Hello

 

We have installed NX11.0.2 MP2 and we have the same behavior.

Is there a setting that the dimensions don't change there position when we move a view?

 

thanks for help

Re: Move view, dimensions change position

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

Lest I assume...

You HAVE checked that the dimensions that move are not positioned (dimension origin) relative to objects (e.g. other dimensions) that are not associated wit the view?

Ken Akerboom Sr CAx Systems Engr, Moog, Inc.
Production: NX10.0.3.5 MP16/TC11.2
I'd rather be e-steamed than e-diseaseled


Re: Move view, dimensions change position

Valued Contributor
Valued Contributor

Hello

 

Weird thing.
This morning I opened the same drawing again and everything was ok...

 

Thank you anyway