Cancel
Showing results for 
Search instead for 
Did you mean: 

Moving Multiple Part In Assembly

Creator
Creator

Hi,

 

How can we check moved part position in assembly with x,y,z co-ordinates and Rx,Ry,Rz angle in NX-10.

 

Is there any option is available (like catia v5 translate and rotate command)

 

 

 

 

9 REPLIES 9

Re: Moving Multiple Part In Assembly

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

You can use information -> object and pick the component. The coordinates and rotation matrix will be shown in the information window. You can find a journal here that will convert the rotation matrix to angles about the X, Y, and Z axes.

Re: Moving Multiple Part In Assembly

Creator
Creator
Hi all
Thanks for your reply but

This is not what I want.

I am not a programmer I am just a NX designer.
What my requirement is
Is there any command is available which shows x,y,z co-ordinates and
rotation angle of the component.
By using information command it only shows the x,y,z co-ordinates.it does
not show's the angle of the component.

Please suggest how can i get it

Re: Moving Multiple Part In Assembly

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

Follow the link in my previous post, copy and paste the code into a new text file, save the text file in a convenient location with the extension .vb. In NX, go to tools -> journal -> play and browse to the file that you saved, press run journal.

 

NX reports the rotation matrix, not the Rx, Ry, and Rz angles. The journal code will convert the rotation matrix to Rx, Ry, and Rz angles for you.

Re: Moving Multiple Part In Assembly

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

Here is a version of the journal attached for your convenience. I could not directly upload a .vb file, you will need to remove the .txt extension from this.

Re: Moving Multiple Part In Assembly

Creator
Creator
thanks a lot cowski1
Highlighted

Re: Moving Multiple Part In Assembly

Creator
Creator

Hi 

 

When i running this it shows some error please see attached image.

 

Thanks,

Bishnu

Re: Moving Multiple Part In Assembly

Creator
Creator

It is working now thank you so much for your support.

 

One more thing i need to ask

how could i move a part or assembly in some co-ordinate and angle.

 

Refer image for your reference.

 

This option is available in catia but i didn't get this option in NX.

please let me know any command is there or not.

 

or any other way which we can use.

 

thank you in advance

 

Re: Moving Multiple Part In Assembly

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

In the move component command, there is a motion option called "delta XYZ"; this option will allow you to key in values for the X, Y, and Z translations, but there is no option for rotation. You can use the angle motion to pick/specify a vector to rotate about and key in an angular value. If you want to specify all the translations and rotations from a single interface, your best bet is to use the "dynamic" motion option. Using dynamic, a large XYZ triad will appear in the "specify orientation" step; click on one of the coneheads and key in a value for translation, or click on one of the spheres between the vectors to key in a rotation. For instance, if you click on the sphere that connects the X and Y vectors, this will rotate the component about the Z axis; you can drag on the sphere handle or key in an exact value in the input box that appears.

Re: Moving Multiple Part In Assembly

Creator
Creator
Hi,

I always use dynamic only to do the same. But I need like where I can enter

X-
Y-
X-
and
Rx-
Ry-
Rz-
Then ok and it goes to respective position at one click.

Can I have journal for this.
If you could help me then it would very helpful for me.

By using dynamic one by one we need to enter sometimes it's getting
confusion.

Thanks
BISHNU