Cancel
Showing results for 
Search instead for 
Did you mean: 

Moving face with threaded hole

Genius
Genius

When I use syncronous technology to move a face that contains threaded holes, the face keep the holes but the thread doesnt move so I have some milimeters without thread at the beginning of the hole. Is there a way to avoid that?

2 REPLIES 2

Re: Moving face with threaded hole

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

Try reordering the "move face" feature before the "hole" (and/or "thread") features.

Re: Moving face with threaded hole

Siemens Phenom Siemens Phenom
Siemens Phenom

As far as features are parametric, you should reorder the hole feature as @cowski1 mentioned.

 

There is a workaround for the same. But seems that it works only in a specific way (If hole depth reduces due to move face command. Limitation??). After using the move face command, either do 'Update for External Change' or 'Feature Playback'. This will also work if faces of the threaded hole are moved. Thread arc will get update after feature playback/update for the external change.