10-02-2017 10:15 AM - edited 10-02-2017 11:12 AM
Good morning all,
I attached three images showing example assembly structure in assembly navigator and a parts list. We're trying to use nested assemblies functionality in parts list to create multi-level / tooling parts list. (Select qty column, right click, settings, column, include nested assemblies)
Basically we would like to have single parts list that contains multiple quantity columns, each for a different assembly. It seems like "Nested Assemblies" functionality is just the thing, but we're not able to set it so that each qty column only lists quantities for selected assembly components, but not its sub-assembly components.
As you can see below "assy0" contains qty 1 of assy1, qty 2 of assy2, and qty 3 of assy3 - we would like to see only those quantities in the "QTY ASSY0" column. We can achieve that by selecting "Top Level Only" in "Edit Levels" of the parts list, but then we're missing the quantities for nested assemblies...
Is there a way to set "Top Level Only" for each column separately to get output like in the third image?
Thanks for any help...
"Top Level Only" off
"Top level only" on
What we want (created in paint)
10-03-2017 02:02 PM
Hi @Voytek,
It appears that your options are:
By default Parts Lists have an option to highlight a cell with a manual edit, you can turn this off by editing the Parts List Settings and unchecking "Highlight" in the 'Manual Text' section.
The functionality requested in ER 6063309 is very similar to your requirements, so consider contacting your local GTAC office to have yourself added to that ER.
Regards, Ben
10-03-2017 04:13 PM - edited 10-03-2017 04:14 PM
10-03-2017 04:30 PM
Hi @Voytek,
I believe this issue (with nested assemblies returning incorrect quantities) was captured in ER 6945857. The same workarounds apply as before.
Regards, Ben
10-03-2017 05:24 PM - edited 10-04-2017 10:22 AM
Yes, the workaround you mentioned works (multiple parts lists), it just splits related assemblies into multiple sheets, where it's sometimes nicer to keep it on one sheet when they're simple enough.
We also have another workaround where we add each assembly and it's sub-assemblies directly to the drawing file and select them from over there instead of from the master assembly. If we do it like that and select "top level only" it works as we want it, but it multiplies the amount of assemblies in drawing file which slows things down on big assemblies.
So yeah... This doesn't shut us down and actually works much better than what we did before (doing the parts lists manually in excell), but still it would be bit simpler / user friendly if nested assemblies functioned as intended.
Thanks.
10-04-2017 10:27 AM
BTW I was able to find ER6063309 in solution center, but not ER6945857. Am I looking in the wrong place?
10-04-2017 10:44 AM