Cancel
Showing results for 
Search instead for 
Did you mean: 

Multiple/Additional weld leaders ?

Genius
Genius

Hi

Is there a way in weld symbol's options to add multiple/additional weld leaders(=arrows) ?

  • Other than just adding blank/empty notes...Smiley Happy

multileader.jpg

2 REPLIES 2

Re: Multiple/Additional weld leaders ?

Siemens Phenom Siemens Phenom
Siemens Phenom

Yes, you can create multiple unique leaders on either side of a weld symbol. See the attached image, which was created in NX 10.

 

You have to use the options in the Leaders group of the Weld dialog box to create unique leaders.Here's an example of how to create different leaders for a symbol. You can apply the same technique to weld symbols too

 

https://docs.plm.automation.siemens.com/tdoc/nx/10.0.3/nx_help/#uid:index_drafting:id1378722:id70165...

 

 

 

Re: Multiple/Additional weld leaders ?

Siemens Phenom Siemens Phenom
Siemens Phenom

Hi,

Yes it should be possible to add multiple leaders to the weld symbols. Attaching a movie herewith. Hope this is what you want.

Regards

Kapil