Cancel
Showing results for 
Search instead for 
Did you mean: 

Multiple Coordinate system rotate using spreadsheet in nx

Experimenter
Experimenter

i need to model a cutter head for dredging and for that i need to rotare a N number of coardinate systemm to a curved curve is there any command to rotate the CSYS with spreadsheet. (in pro-e there is a table command to rotate the all the cooardinate system )   

2 REPLIES 2

Re: Multiple Coordinate system rotate using spreadsheet in nx

Siemens Phenom Siemens Phenom
Siemens Phenom

Hi @Mohanty ,

 

Welcome to Community!!!

Can you please add an image?

Regards,
Samadhan

GTAC | NX Help: NX1102 | NX1202 | NX1847
Please mark post as an "Accepted Solution", if it answers your question/is more helpful!

Re: Multiple Coordinate system rotate using spreadsheet in nx

Siemens Phenom Siemens Phenom
Siemens Phenom

Hi @Mohanty ,

Try using 'pattern feature'. Toggle ON 'Use spreadsheet' and define the parameters.

Thanks,

Amol