Cancel
Showing results for 
Search instead for 
Did you mean: 
Highlighted

Multiple Datum Coordinate systems(1,2,3) in drawing ?

Genius
Genius

Hello

Why NX creates Multiple Datum Coordinate Systems(1,2,3) in drawing ?

  • They turn View Borders large and when I delete them the borders turn to normal size...
  • So is it ok and problem free to delete all the Datum Coordinate Systems(1,2,3) ?

borders.jpg

3 REPLIES 3

Re: Multiple Datum Coordinate systems(1,2,3) in drawing ?

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

If they are not used in the drawing and they are not needed for a downstream operation, they can be deleted.

Re: Multiple Datum Coordinate systems(1,2,3) in drawing ?

Siemens Esteemed Contributor Siemens Esteemed Contributor
Siemens Esteemed Contributor
Or just right click on them and choose Hide.

Re: Multiple Datum Coordinate systems(1,2,3) in drawing ?

Honored Contributor
Honored Contributor

If they have some use, which prevents you from deleting them, you could move them to some other (empty) layer, and then make that layer invisible in the drawing views.

-Dave
NX1867(if it had versions) | Teamcenter 11.6 | Windows 10