Cancel
Showing results for 
Search instead for 
Did you mean: 

Multiple Lines in one cell

Experimenter
Experimenter

Hey All,

 

New here and have a quick question, in NX10 I'm trying to update the title block and need to add the company location under the company name. I want to do this in the same cell but can't figure out the modifier to give me a carrage return. I tried COMPANY NAME <BR> (like HTML) but that didn't work. I looked in the Command Finder and couldnt find anything useful. I don't want to open it in a spread sheet as thats a little over kill. A google search has been fruitless. Any one know here I can find a list of cell modifiers I can save for referance? 

 

Thank you for the help.

2 REPLIES

Re: Multiple Lines in one cell

Solution Partner Phenom Solution Partner Phenom
Solution Partner Phenom
You can only do it when it's at the tabular note stage, before adding to or when it's removed from a title block. Right click in the tabular note cell and choose Edit --> Text. You can then use the note editor to put in a new line.
Anthony Galante, Senior Support Engineer
PhoenxPLM
24 versions of NX installed: NX4 to NX12, plus TC11.2

Re: Multiple Lines in one cell

Esteemed Contributor
Esteemed Contributor

When programming in C++, I can force a line break by using "\n" in the string

Not sure how this translates to interactively filling in the value

Ken Akerboom Sr CAx Systems Engr, Moog, Inc.
Production: NX10.0.3.5 MP5 + patch/TC11.2
I'd rather be e-steemed than e-diseaseled